EGEAR.PULSESIN

Description

EGEAR.PULSESIN is the number of encoder counts the motor moves for each EGEAR.PULSESOUT number of position counts. EGEAR.PULSESIN must be set more recently than EGEAR.RATIO in order to use exact electronic gearing.

General Information

Type

R/W

Units

Motor revolutions / Encoder Revolution

Range

0 to 65,535

Default Value

1

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1070

No 16 bit No

M_01-05-11-000

Related Topics

MOVE.MOVING | EGEAR.ON | FB2.SOURCE | FB2.ENCRES | FB2.MODE